MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hello Stagiaire I built the same Cubemos example in a new Unity project and had the same problems with finding a model. The 30 day free trial period that I had on the Skeleton Tracking SDK has ru...
-
RealSense cameras are a Class 1 laser product that are designed for safe use in industrial applications. Full regulatory information for the product range can be found in the link below. https://w...
-
There can be differences between different Windows versions and between different computers in how the SR300's driver details are handled. for example, one PC might put all the SR300 drivers under...
-
In general it is fine to post RealSense questions here instead of the GitHub. The exceptions are feature requests or RealSense T265 questions - those should be posted on the GitHub. If the questi...
-
I apologise for the delay in responding further. Each RealSense camera product has an individual product ID number. This may cause problems if an old program is specifically looking for the SR300'...
-
The SR305 has an SR300 camera circuit board inside. Essentially, it is an SR300 with a new outer casing that makes it easier to mount than the original SR300 model. My own old SR300 identifies it...
-
If you are using the script above, it is not meant for use directly in MATLAB. Eliza was suggesting to modify it for MATLAB. If you are aiming to use a RealSense 400 Series camera with MATLAB, the...
-
The new RealSense L515 lidar depth camera can analyse 23 million accurate depth points per second and does not need to be calibrated during its lifespan. It can also provide a per-pixel confidenc...
-
There is a Unity implementation of OpenCV in the Unity Asset Store, though it is not inexpensive and I could not make guarantees that an OpenCV DNN program would work in it. https://assetstore.unit...
-
Thanks for the effort that you have put into debugging this problem! I do not have information on unpack_z16. I notice though that in the Viewer you are getting a warning message about multiple ud...