MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The problem can have more to do with the stability of the power supplied to the port than the amount of power, and RealSense cameras are sensitive to the state of the port. Mains powered hubs typi...
-
In the Windows privacy settings, can you check please that permission for apps to access the camera is set to On. The link below explains how to do this check. https://github.com/IntelRealSense/li...
-
In the "Controls" section of the RealSense Viewer's options side-panel there is an option called 'Laser Power'. Could you set it to '0' whilst the camera is not streaming please and then activate ...
-
If you are using a 400 Series camera such as D415 or D435, accuracy increases as resolution is increased. This is because the Stereo (left and right) depth sensing technology in the 400 Series der...
-
Windows 10 Home should be fine. It is what I have on my personal workstation that I use with RealSense SR300, D415 and D435i.
-
Windows 7 supports D415 and D435. The D435i does not yet have Windows 7 support. It could be provided in a future SDK release. My interpretation of information about Windows 8.1 is that it would ...
-
If you want to try manually updating the firmware with a firmware file (with the Viewer's 'Update Firmware' menu option or with the rs-fw-update tool), one of the RealSense developers offers advice...
-
SR300 Depth Module Kits should behave like the SR300 Developer Kit camera. The difference is that the SR300 Depth Module Kit is a camera on a circuit board without an outer casing or USB connector...
-
Hi Alphatozeta If you are loading .ply point cloud files into 3D software such as CloudCompare or MeshLab, you may experience problems with the scaling of the cloud if the depth units scale of th...
-
Thanks so much for posting your solution. I'm really pleased that Cubemos were able to help you. Good luck with the software!