MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Pratik The On-Chip Self Calibration system of the 400 Series cameras has a 'Health Check' function that can monitor the metrics of a camera over time. The self calibration system is fast and, unl...
-
Hi Glaceonw The D415 can track motion at human walking pace, so it should be able to cope fine with a plant in a slight breeze. For fast motion (including a vehicle travelling at full speed), the...
-
The other site would have to re-record the footage. An unusual characteristic of this case is why post-processing settings that were active during the recording would matter at all. This is becaus...
-
Dorodnic the RealSense SDK Manager has said that the dots are most likely to appear on the color image when doing short-range sensing, due to laser emission being significant at that short distance...
-
The RealSense SDK does have a tool called rs-convert for converting a bag to other formats, if the tool could access the bag when the RealSense Viewer cannot import it. https://github.com/IntelReal...
-
Evan M Mitchell Thanks so much for sharing confirmation of what worked for you with the RealSense community!
-
Hi Jallanhall The Zero Order Filter is a depth "post-processing" filter specific to the L515 that was added in SDK version 2.31.0 and is set to 'On' by default. 'Post-processing' means that it is ...
-
Hi Federico Frontali I have replied on the GitHub version of this question. Thanks! https://github.com/IntelRealSense/librealsense/issues/6525
-
RealSense cameras are a Class 1 laser device and do not interfere with each other (their fields of view can also be overlapped without problems), so the likelihood of damage from observing each oth...
-
Hi Shipbrook I sincerely apologise for all the trouble that you have had. Could you please send an email to sys_support@intel.com about this case so that it can be resolved through email. I will...