MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi, what computer / computing device are you trying to do a pip3 install on please?
-
1. The 400 Series cameras are Stereo depth cameras. The T265 does not have depth sensing capability and has to be paired with a depth camera such as a 400 Series stereo camera if you want to perf...
-
UYVY is not the same as Y16. The image below shows the range of IR formats that are selectable in the RealSense Viewer. Documentation of the configuration of each RealSense stream format is ...
-
On the 400 Series cameras, the IR imager can also provide a color stream in addition to the dedicated color one provided by an RGB imager. In fact on the D415 model, the RGB and IR imagers use the...
-
You are very welcome. Good luck!
-
You could set up an ethernet network, with the board with the camera attached being the 'server' and the board without a camera being the 'client'. The process is described in Intel's white-paper ...
-
A way to get around the technological limitations may be to purchase a physical optical filter and position it over the camera lens. The Intel paper on the subject in the link below was designed f...
-
The issues that you describe are related to the physics of depth sensing cameras (not just RealSense). Dark surfaces such as black / dark grey are difficult for the camera to read depth detail fro...
-
The F200 was five years ago, so I'm having to search my memory about its use with OBS. My recollection is that it was intended to be used with the "green screen" background removal feature of OBS,...
-
I believe that on the F200, the driver that would provide video on a non-RealSense program would be the Virtual Driver. Can you check please if you are able to change the selected driver from Dept...