MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Although the D415 has around 2x the image quality of D435, it has a minimum distance of 0.3 m instead of the 0.1 m of the D435. So you would need to adjust the Disparity Shift to reduce the D415's...
-
Regarding not having enough points to measure on the rod: if the depth data in an image is too low (too "sparse") then you can reduce sparseness by increasing the value of the Laser Power option. H...
-
If you are building librealsense with CMake, you may get a performance boost if you include the term -DCMAKE_BUILD_TYPE=release if you are not using this term already.
-
Hi 819765928 There does not need to be a value inside the brackets of wait_for_frames(), as this instruction just means "wait until a complete frame is received instead of instantly processing fram...
-
If the goal is to measure the diameter of the top of the rod / bolt, I wonder if the complexity of a point cloud is necessary when 2D mode may be able to accomplish the same measurement using the t...
-
Changing the Depth Units Scale has the most effect when doing close-range sensing, I believe. So it may be worth trying to reduce the depth units from their 0.001 default to the 0.0001 minimum.
-
If you are experiencing the same issue on multiple computers, then it narrows the most likely options down to: - A faulty USB cable that cannot cope with streaming high volumes of data - Faulty f...
-
The subject of point cloud "ghost noise" is discussed in the link below. https://github.com/IntelRealSense/librealsense/issues/4553 Advice about reducing such noise is given here: https://github.c...
-
Are you using with the camera the official short USB cable supplied with it, or are you using your own choice of cable that is longer, please?
-
Shiny surfaces are tricky to deal with if you cannot apply anything to the bolts. If you could, then you could have used a professional 3D scanning spray on them that is used for situations such a...