MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Tracking of head turning via "landmark" points around the eyes was possible for SR300 with the old 2016 RealSense SDK for Windows, which is obsolete and no longer updated or supported. https://soft...
-
Hi Emmanuel. At very close range I don't think you will get much benefit from changing cameras, as the error factor starts at near zero at the camera lens and increases linearly over distance. So...
-
Hi Andre I see that you have also posted your question on the RealSense GitHub. Please await an answer there at the GitHub, as this forum does not handle T265 related questions. Thank you very m...
-
1. A PCIe card may make a positive difference compared to using built-in ports if you choose one with a connector that allows an additional 5V of power can be delivered to the card by the computer...
-
rs-capture is a program that should launch when double-leftclicked on. Are you able to run the realsense-viewer program please? If that also does not launch, it would suggest that your computer's...
-
Hi Imutlu07 If you are tracking objects and will be using RGB and you will be using multiple cameras, I would recommend the new RealSense D455 stereo camera. https://github.com/IntelRealSense/lib...
-
Hi Shlomi Shoshani. The officially recommended supplier for USB-C cables for the 400 Series cameras in the cameras' Intel data sheet document is a company called Newnex. They can provide industri...
-
You are very welcome. I'm pleased that I could help. :)
-
I note that you are in "3D" mode in the top corner of the Viewer. This is for generating a type of depth scan called a Point Cloud. If you click on the "2D" button in the corner then you will see...
-
It is a bit difficult to see what is in the kindly provided image. If you have a lot of black or dark grey surfaces in the scene (such as a black office chair), the camera will find it hard to rea...