MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I researched this case extensively from the beginning to look for new possibilities to follow, but did not find much. My feling is that at this point, the best path to follow may be: 1. Download ...
-
The type of SLAM used with SR30x cameras would be RGB-D SLAM because its sensing technology is based on coded light / structured light, rather than the Stereo sensing of the 400 Series cameras. Th...
-
Great news that the driver re-installation worked for you! Thanks very much too for your kind words of service review. :)
-
Apparently Microsoft hid the Hardware and Devices part of the troubleshooter. To access it now, you have to open the Command Prompt interface and copy and paste the line below into the Command Pro...
-
You are very welcome. :) It is rarely a good sign when a device ends up under Other Devices or some such other general category though, as it can indicate a problem with the installed drivers. You...
-
The actual camera drivers should be under the Camera category of the Device Manager if they have been installed correctly. Can you check to see whether they are there please? Having said that, ...
-
It may be useful for you to watch Intel's 44 minute seminar on YouTube about using T265 and D435 together (see the 17 minutes 15 second point for the start of the part where the two together are di...
-
Librealsense can sense through glass. Intel published a tutorial for the Python language on sensing through aquarium glass. https://github.com/IntelRealSense/librealsense/blob/jupyter/notebooks/de...
-
T265 questions such as your V-SLAM one are handled on the RealSense GitHub forum. You can post a question involving T265 there by visiting the link below and clicking the New Issue button. https:/...
-
I am guessing that you downloaded the Intel.RealSense.FW.Update.exe file from the Assets file list on the RealSense SDK Releases page? https://github.com/IntelRealSense/librealsense/releases/tag/v2...