MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Eidsonbrandon I would recommend following the version of the Mac instructions in the link below, as they are the ones linked to from the front page of the librealsense GitHub site and so will b...
-
You can test the RealSense SDK camera software without having a camera. Once the SDK is installed, you can drag and drop a sample bag file into the central panel of the RealSense Viewer program...
-
I understand your situation. I answered a case involving blurring when scanning barcodes at 70 cm range on the RealSense GitHub forum just now. https://github.com/IntelRealSense/librealsense/issue...
-
Hi Baltabai K The IR Emitter on the 400 Series cameras projects a pattern of semi-random dots onto a scene to aid the camera in analysing depth detail from surfaces that the dots are cast upon. I...
-
The D415, D435, D435i and D455 camera models have an infrared projector component in them that is separate from the left and right IR sensors. Yes, it is also known as the IR Emitter. Is the tab...
-
The Depth + Tracking bundle in the RealSense Store certainly is a valid way to get a D435 and T265 together in the same bundle. The T265 has the same IMU component inside it that the D435i does, so...
-
Hi Barry Somers Having texture for the camera to analyse is important when sensing flat surfaces such as doors, walls, desks, etc. If the object has no texture or low texture then you can provide...
-
Hi Thedavidgabriel I considered your use-case carefully. I believe that in this case, the L515 may be unsuitable. Homes tend to have variable lighting and shadow, instead of a consistent light so...
-
I'm actually thinking now that what could make the most difference is to look at Intel's white-paper document on improving depth data on outdoor drones. It has some excellent improvement advice th...
-
1. It is difficult for Intel to correct a problem in RealSense cameras that is being caused by something in the Windows operating system.. 2. SR300 should be able to function as a webcam in vide...