MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Although F455 and D455 have similar naming, they are very different products.
-
Hi Roman Abrahamson There is not a CAD file available for the D421 depth module board, unfortunately. Its measurements are 95 mm (W) × 32 mm (H) × 10.18 mm (D) so you could use that information...
-
Hi Mauriello When performing hardware sync with an external trigger signal, it can be difficult as the generated signal has to have a frequency that is matched very closely with the FPS of the cam...
-
RealSense ID is available to purchase now from the Store if you are interested in them. :)
-
Hi Nguyenthuu30031999 This message about pre-ordering is over a year old and RealSense ID is now in stock in the official RealSense Store. Yes, the models in the Store are the same ones on the fac...
-
Hi Westclyde644 I believe that your only option for suppressing that one specific message type would be a suggestion from earlier in this discussion to edit line 42 of the librealsense source code...
-
Hi Parthijaya73 To receive assistance with your GMSL issue, please create a private support ticket on Intel's Zendesk support channel like Dp above did so that a RealSense team member can advise you.
-
Hi Vito Plahuta I do not have information on this subject but in general, SDK code may reference model names that are not yet available but it does not mean that it will be released as a product. ...
-
As the problem is apparently specific to your computer (as it worked on your friend's computer that had not been updated), you could next try updating your computer's graphics driver. Open the Wi...
-
I would expect the libuvc installation script to continue to work with a computer that it has previously worked on but do not currently have information regarding how a librealsense build based on ...