RealSense Support

Unable to find D421 CAD file

Comments

1 comment

  • MartyG

    Hi Roman Abrahamson  There is not a CAD file available for the D421 depth module board, unfortunately.   Its measurements are  95 mm (W) × 32 mm (H) × 10.18 mm (D) so you could use that information to create a simple representation of the shape of the module in a newly created CAD project.

     

    If your project does require an entry level depth module and you need CAD files, a two-board alternative to D421 you could consider that does have CAD files is a D430 depth module and a Vision Processor D4 V1 board.  This combination will be equivalent to a D435 camera, except it will not have an RGB sensor.

    0
    Comment actions Permalink

Please sign in to leave a comment.