MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Incron13 The standard procedure for building the set of examples would be to use CMake and include the build flag -DBUILD_EXAMPLES=TRUE in the CMake build statement. If an individual example ...
-
Intel has a white-paper document about using projectors that provides information about selecting and using external projectors. https://dev.intelrealsense.com/docs/projectors
-
Hi Lghasemz The SR300 / SR305 has a single infrared stream, whilst the 400 Series cameras have a pair of left and right streams (which is why the 400 Series is called a Stereo depth camera). When ...
-
Hi Baltabai K The subject of how the Depth Quality Tool references plane fit is discussed in the link below. https://github.com/IntelRealSense/librealsense/issues/3866
-
Hi Vinicius Ramalho There can be different forms of the ghost noise phenomenon. For your particular case, I would first recommend reading the discussion in the link below. https://github.com/Inte...
-
Hi Rogerwgardner41 When you say that your SR300 is 'built in', do you mean that it is built into a device such as a tablet or laptop please instead of being attached to a computer with a USB cable...
-
Hi Sylvain I considered your question very carefully. You can access the camera hardware directly using callbacks to the Low-Level API of the RealSense SDK. https://github.com/IntelRealSense/libr...
-
You can export the settings in the RealSense Viewer to a preset configuration file called a JSON. This can be done using a button near the top of the options panel. RealSense Viewerの設定を、JSONと呼ばれ...
-
Laser Auto is a deprecated feature that I understand was originally designed to toggle the emitter on and off. Intel later added a mode to alternate the emitter on-off on a per-frame basis, though...
-
Hi Ajg206 The 'average' Laser Power of 150 mw represents a default value, and is set as the default value for the changeable Laser Power option in the RealSense SDK's RealSense Viewer program. In...