MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If you are using Linux than please tell me and I can help you with instructions for installing the 2.39.0 SDK. If you are using Microsoft Windows then you can install SDK 2.39.0 by visiting the lin...
-
Hi Kweon9612 You do not need to have the UWP driver installed in order to use RealSense with Windows. The driver provides an interface between RealSense and products that support Microsoft's Univ...
-
Yes the D4 is always active. Although the D4 can do some of the processing work, having a good computer specification does make a positive difference, especially for functions that are processing ...
-
Hi Hdasilva1967 Are you using the RealSense Viewer program please? If you are, it sounds as though you may have activated Fullscreen mode. If this is the case, pressing the F8 key on the keyboar...
-
Intel's RealSense official blog article about the use of D435 on Everdrone emergency medical drones is also worth reading. https://www.intelrealsense.com/everdrone/
-
Hi Bgarby The D435 has been used successfully on drones, yes. The links below should be a good place to start in seeking solutions to your drone false-depth issues. https://github.com/IntelRealSen...
-
Translation: Regarding how different CPUs of PC computers affect the rate at which camera images are acquired. With a resolution of 640x480 on my desktop computer, the number of frames is up to 50...
-
Translation:. Why do I get the following error? Also, please tell me how to solve it. Invalid Value in rs2_create_device(info_list:0E43DA88,index:0):set_xu(ctrl=1)failed!Last Error:Bad file descri...
-
Hi Hanme Kim. This is not a fault or bug and the D455 does not need to be returned. I will refer your case to a member of Intel who can provide specialist advice about this issue.
-
Yes, you would still need to deliberately align depth and color with code on D455. The changes with D455 in regard to alignment are to do with its hardware design rather than the way in which it i...