MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Chutchinson The D435i stereo depth camera model does not have built-in support for pose stream data like the T265 Tracking Camera model does. If you want to obtain pose (position + angle) of ...
-
Hi Lamlk1341 This tinting phenomenon is a known characteristic of the D455 model under certain lighting conditions and is not a fault. If you click on the link below to launch a download of the S...
-
Hi Conrad RealSense camera technology should be able to meet your requirements. The L515 lidar depth model would not be suitable for your project though as it is suited to indoor use under contro...
-
Hi Gmg718 You could generate a point cloud in the free RealSense tool called the RealSense Viewer and export the point cloud as a .ply format file. That ply could then be imported into a free ope...
-
Hi Lschreurs25 The projector component on the D435 model pulses in time with exposure, whilst on the D415 model the projector is always on. So I would first recommend confirming or eliminating th...
-
5.10.6 was the recommended firmware for the RealSense SDK version 2.17.0 from November 2018. https://github.com/IntelRealSense/librealsense/releases/tag/v2.17.0
-
The D455's optimal depth accuracy resolution is 848x480, so I would recommend using that. If you would prefer 1280x720 though then you could try using it in combination with the High Accuracy came...
-
Hi Jianfei Li A statement about RealSense camera MTTF / MTBF is provided on this support site. https://support.intelrealsense.com/hc/en-us/articles/360056072433-What-is-the-Mean-Time-to-Failure-of...
-
Hi Karthikeyan Yuvraj Multiple RealSense 400 Series cameras do not interfere with each other.
-
Excellent! Thanks very much for the update about your success :)