MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I note that you have "RGB Module Depth" highlighted in the image above. Does it also fail with RGB Module RGB selected? On some non-RealSense video applications, a RealSense camera may also fail...
-
In regard to accuracy: assuming that the camera is less than 3 meters from the observed object, setting the Medium Density camera configuration preset will give a good balance between accuracy and ...
-
Hello, the RealSense SDK has a Python example program called box_dimensioner_multicam that works with a single camera despite the name. After the program is launched, the object to be measured is ...
-
Thanks very much. Please create another new issue for that support ticket request using the New Post button on the forum front page. Good luck!
-
You are very welcome, Danieldach22 - I'm pleased to hear that they were useful for you too!
-
Hi Hoyeneyi Have you set the Inter Cam Sync Mode of one of the cameras to be Master (Inter Cam Sync Mode '1') and set the other to sync to it as a Slave ('2') please? Also, if hardware sync is w...
-
Hi W Si The RealSense SDK release notes for the 2.50.0 SDK version have a link to the focal-length and tare target in PDF format. This PDF is configured for 8.5x11" dimensions. https://librealsen...
-
Hi Ronghao Jonathantan There is a past discussion about a range of possible ways to segment out a mannequin from its background at the link below. https://support.intelrealsense.com/hc/en-us/commun...
-
The D435i would not be a suitable choice of camera model for tracking the linear velocity of the device. The RealSense T265 Tracking Camera would be the appropriate model choice for obtaining real...
-
Hi Stafangagkub There has only been one previous case (in the link below) in December 2021 about using RealSense with a Simulink S-function and it did not have a clear solution at its outcome. htt...