MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If you are encountering scenes where there is problems with exposure because there are simultaneously areas of brightness and areas that are dark in the same view then enabling the SDK's High-Dynam...
-
1. I do not have a T265 to test with at my location as others handle T265 related cases. I can point you towards some useful references for using a T265 and 400 Series camera together though. T...
-
It's great to hear that you have been successful. Thanks so much for sharing your HDR knowledge in such detail with the RealSense community :)
-
Hi Srikar Namburu Are you capturing a single frame, please? If you are and you have auto-exposure enabled then the exposure can take several frames to settle down after the camera pipeline is sta...
-
The D405 is designed for close-range, high accuracy sensing with an ideal depth measuring range of 7cm to 50 cm so it would not be a suitable choice if you are going to be depth-sensing objects or ...
-
Pausing the live stream will not prevent multiple frames from being recorded to a bag file. The best chance of capturing a single frame in the Viewer with your quick stop-start technique may be to ...
-
The D435f will not cut out the multiple white dots of the infrared pattern if that is what you mean. The D405 does, shown in the same scene observed with a D405. Like your own scene, I placed a D...
-
For comparison I observed a scene with a D435i (upper image) and D435f (lower image). The most notable difference was that on the D435f image the illuminated image on the laptop screen was not vis...
-
The filters on the D405 and D435f camera models have different purposes. The D405's filter is IR Cut which blocks infrared light frequencies and so makes the IR dot pattern invisible to it. So a ...
-
Thanks very much. I look forward to your next report. You could also test whether setting the Advanced Mode option Second Peak Threshold to zero reduces the depth pulsing, as described at the li...