RealSense Support

Issues with depth frame quality on Intel Realsense D415

Comments

3 comments

  • MartyG

    Hi Srikar Namburu  Are you capturing a single frame, please?  If you are and you have auto-exposure enabled then the exposure can take several frames to settle down after the camera pipeline is started.  This can result in incorrect exposure on the first couple of frames.

     

    If you are writing your own program script then a simple way to avoid this issue is to use a 'for' instruction to skip the first several frames before commencing capture.  Code snippet examples for doing so are shown below.

     

    C++

    // Instruct pipeline to start streaming with the requested configuration

    pipe.start(cfg);

    // Camera warmup - dropping several first frames to let auto-exposure stabilize

    rs2::frameset frames;

    for(int i = 0; i < 30; i++)

    {

    // Wait for all configured streams to produce a frame

    frames = pipe.wait_for_frames();

    }

     

    Python

    profile = pipe.start(cfg)

    # Skip 5 first frames to give the Auto-Exposure time to adjust

    for i in range(5):

    pipe.wait_for_frames()

     

    **********

     

    If you are capturing a continuous live stream instead of a single frame and are experiencing exposure problems then please let me know.

    0
    Comment actions Permalink
  • Srikar Namburu

    Hi MartyX Grover Thank you for quick reply. 

    I am capturing a continuous live stream. 

    0
    Comment actions Permalink
  • MartyG

    If you are encountering scenes where there is problems with exposure because there are simultaneously areas of brightness and areas that are dark in the same view then enabling the SDK's High-Dynamic Range (HDR) exposure control may help to deal with it.  Intel have a white-paper guide about the subject at the link below.

    https://dev.intelrealsense.com/docs/high-dynamic-range-with-stereoscopic-depth-cameras

     

    Under-exposure and over-exposure is discussed in Section 2.3 of the guide.

    https://dev.intelrealsense.com/docs/high-dynamic-range-with-stereoscopic-depth-cameras#23-under-and-over-exposure

    0
    Comment actions Permalink

Please sign in to leave a comment.