MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Bruno M Cebola This question has been responded to at the link below. Thanks! https://github.com/IntelRealSense/librealsense/issues/12721#issuecomment-1975370865
-
Your situation sounds like a past case at the link below where the sides of a box on the image were not 90 degrees even though the box in the real world was 90 degrees. https://github.com/IntelReal...
-
Hi Thomal2002 You can list the intrinsics for a specific RealSense camera (including the distortion model used by each stream type) using the calibration information mode of the RealSense SDK's rs...
-
The best way to achieve your goal may be to apply a post-processing filter in the RealSense Unity wrapper, such as the Threshold filter that allows you to define a minimum and maximum distance for ...
-
Hi Tony00013 I tested the D435f camera model with a bag of almond nuts similar in structure to your model. Though the almonds were larger than 5 mm in size, the camera was unable to distinguish i...
-
Hi Vijaykumar Shejal The RealSense Viewer and firmware driver versions that you are using date back to end 2018 / start 2019, and USB connection problems were more common back then before fixes we...
-
Yes, with set_option instructions '1' enables an option and '0' disables it. Setting Auto Exposure Priority to '1' will not improve depth accuracy. Setting Emitter Enabled to '1' and the Visual ...
-
Hi Saadisaadi1 The RealSense SDK operates on rules called the Multi-Streaming Model that dictate that two applications cannot simultaneously access the same stream on the same camera. So if Unity...
-
Hi Dan Pittsley The current version of the Jetson installation instructions can be found at the link below. https://github.com/IntelRealSense/librealsense/blob/master/doc/installation_jetson.md ...
-
Hello, this support forum is for Intel RealSense camera products. For a CPU question, I recommend posting it at Intel's Processors support forum at the link below. Hallo, dieses Support-Forum is...