MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Fpelegri You could reduce RGB blurring on the D435i model by using one of the following methods: 1. If you have auto-exposure enabled, set depth FPS to 30 and RGB FPS to 60. This should com...
-
Hi Mans Ekelund Because 400 Series cameras have a tripod thread hole on their base that has a standardized tripod thread size, a wide range of general mounting devices should be able to be attache...
-
If you cannot set the left infrared to Y8 then this could suggest the possibility of a driver error. If you are using Windows then please try uninstalling and re-installing the RGB and Depth drive...
-
The Windows version of the SDK uses Microsoft Media Foundation as its backend by default. It can alternatively be built from source code with CMake instead of using the automated Intel.RealSense...
-
Hi Ralucadianapetre Did you build the RealSense SDK (librealsense) from source code with the RSUSB backend please? If you did, the RSUSB backend can take longer to register an option change compa...
-
Hi Ralucadianapetre As mentioned earlier in this discussion, the following conditions apply. 1. If you have a USB 2 connection then only the left IR stream can be enabled. 2. If you have a D43...
-
Hi Alal you can find information about the interface that the sensors use by performing a word find operation in the 400 Series' data sheet document (at the link below) for the term mipi csi-2 ...
-
Hi Andrew John Madey You can find a range of research papers about insect counting projects that use Tensorflow by googling the term insects "count" "tensorflow" (making sure to include the quotat...
-
There are a wide range of video guides on the official RealSense YouTube channel. https://www.youtube.com/c/IntelRealSense/videos Of those videos, the guide to the RealSense Viewer would be a goo...
-
Hi Andrew John Madey All of the RealSense 400 Series camera models are stereo depth, because depth is constructed from left and right infrared sensors (hence the 'stereo' term). When switching t...