MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
A possible way to report the time when a trigger is received without syncing timestamps may be to check the status of the metadata parameter RS2_FRAME_METADATA_GPIO_INPUT_DATA to detect whether a c...
-
Hi Fpelegri The dot pattern cast by the projector is semi-random, and how visible the dots are to the camera will also depend on environmental conditions such as lighting and the type of material ...
-
Hi Fpelegri Does the hole close up if you increase the Laser Power setting from its default of '150' to its maximum of '360' please? Increasing the Laser Power can close up holes in the depth ima...
-
Hi Yixun Liu I agree that the D415 camera model would be a suitable choice for the depth sensing range that you have planned. D415 also has around half the depth error over distance (RMS Error) o...
-
Hi Yixun Liu Chessboards are a pattern that is easily recognizable to RealSense cameras as they commonly use that pattern for camera calibration. An example of this is the RealSense Dynamic Calib...
-
Whilst you may be able to obtain depth data up to 20 meters away, it may not have a high accuracy. Depth error is around zero at the camera lens and increases linearly as distance from the camera ...
-
Hi Steve Steve The threshold filter's maximum distance is set to 4 (meters) by default, so when it is enabled a D455 will only be able to render detail up to 4 meters away on its depth image unles...
-
In mode 3 (Full Slave), it is meant to sync both depth and RGB timestamps with the master trigger instead of just depth. In practice though the RGB sync did not work (this paper was an experiment ...
-
Hello, the External Synchronization paper has been withdrawn from the white-paper directory. The reason for this is that its contents were an experimental Proof of Concept that are not validated b...
-
Hi Flawedsoftware For your application the most suitable RealSense camera model is likely to be the D405, which is designed for high accuracy and image quality at very close range. It has an idea...