MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The most important factor will not be the dimensions of the print-out (as it is is going to vary depending on whether A4 or US Letter format paper is used) but instead that the yellow box surrounds...
-
Hi Duke Zacks Infrared 2 is only available on a USB 3 connection. If the camera is plugged into a USB 2.1 port on the computer or it is in a USB 3 port but being mis-detected as a USB 2.1 connect...
-
The Intel guides at the links below provide advice about reducing the impact of the repeating pattern phenomenon. https://dev.intelrealsense.com/docs/depth-map-improvements-for-stereo-based-depth-c...
-
Taking a depth coordinate reading in the RealSense Viewer from the calibration image attached to the ceiling may not work well. This is because it is a general physics principle (not specific to Re...
-
By default the center-line of the left infrared sensor is the depth origin reference-point. If depth is aligned to color then the center-line of the color sensor becomes the origin. The bottom o...
-
Hi Roysaad1 I would add that if you need to build the project from scratch then the RealSense AR projector project at the link below may be a helpful reference, though it is quite old now. https:/...
-
You can activate the RealSense SDK's On-Chip Calibration using Python code instead of accessing it through the RealSense Viewer by using the scripting at the link below. https://dev.intelrealsense....
-
In real-world conditions you may not see a noticable difference between alignment on D435 / D435i and D455. A key area where having the depth and RGB sensors on different PCBs like on the D435 / D...
-
Hi Yixun Liu Most RealSense stream formats are rectified, including Y8 infrared. If you have a 400 Series camera model and a USB 3 connection then the infrared Y16 format is unrectified though, a...
-
Hi Yixun Liu, The source of that quote is Intel's 'Which RealSense device is right for you' camera model comparison article. https://www.intelrealsense.com/which-device-is-right-for-you/ The data...