MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Thanks for the joke, it made me laugh. :) Good luck with the cable!
-
In the few cases I have seen that do specifically mention using a 3.1 Gen 2 USB-C cable with RealSense, the users have reported that the cable worked for them. Here is an example of such a comment...
-
It is not unusual to have variations in the number of frames in a recorded bag. The subject, and the possibility of synchronising streams during the recording process, is discussed in the link bel...
-
I don't know of a direct way to do the conversion. It is feasible as a two-step process though. STEP ONE Use the RealSense SDK's Convert tool to extract the frames from the bag as a set of PNG im...
-
1. Looking at the quoted section in the paper, its mention of Left = High Density and Right = High Accuracy is referring to how the two illustrations are using different Visual Presets to achieve ...
-
Yes, it is possible to sync the D415 and D435. https://github.com/IntelRealSense/librealsense/issues/3836#issuecomment-486421246 RealSense cameras can also be hardware synced with non-RealSense ca...
-
I would not recommend going further back than a couple of versions from the current one when downgrading. In that case, I would suggest trying version '5_12_0_0'.
-
If the RealSense Viewer is working for you then you can upgrade / downgrade the firmware by going to the 'More' icon at the top of the options panel and selecting the firmware upgrade option from i...
-
I researched the subject of segmentation faults carefully. Unfortunately, virtually all previous cases on the RealSense GitHub forum ended without a clear solution (typically because the user stop...
-
The link below gives advice on installing libgazebo7 for different ROS versions. http://gazebosim.org/tutorials?tut=ros_installing&cat=connect_ros#ClonetheGithubRepositories It starts by asking to...