MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I checked the genlock sync white-paper document. It states "The Genlock feature only works on Intel RealSense cameras that are based on Global Shutter stereo imagers. This means that it currently w...
-
The Inter Cam Sync Mode option should display the following message when using the 2.53.1 version of the RealSense Viewer. Can you confirm please that the version number at the top of your Vie...
-
Hi Thermofluid06 I have received information from Intel that it is fine to use the D457 only in USB mode and it has the same USB performance and the same feature-set as the D455, with the added IP...
-
Hi Roman Leuzinger I have received information from Intel that it is fine to use the D457 only in USB mode and it has the same USB performance and the same feature-set as the D455, with the added ...
-
Hi Martin Kambla and Javier and Baris Bilgin I have received information from Intel that it is fine to use the D457 only in USB mode and it has the same USB performance and the same feature-set as...
-
You said earlier in this discussion that "I am trying to change the Inter Cam Sync Mode to 4, but only able to see up to 2". What interface are you attempting to change the value in (such as the R...
-
The depth image is not generated from the left and right depth streams 'Infrared' and 'Infrared 2'. Instead, a depth frame is constructed from the raw left and right infrared frames in the camera ...
-
Thanks so much Marco Pirondini for sharing your knowledge and your code with the RealSense community!
-
If you can still see the dots at minimum laser power and you need the projector to be active so that it provides an IR light source, the only other action that you can likely take is to change the ...
-
Hi Javier Intel recommend using the D457-compatible product by Connect Tech at the link below as a means of testing the D457, as their product has built-in support for D457 and does not require th...