RealSense Support

I created a system based on Intel Realsense D455 and OpenVino 2022

Comments

5 comments

  • MartyG

    Hi Marco Pirondini  Have you seen the RealSense SDK's OpenVINO face detection example program rs-face-vino at the link below which uses the trained model Intermediate Representation files face-detection-adas-0001.xml and .bin please?

    https://github.com/IntelRealSense/librealsense/tree/master/wrappers/openvino/face

    0
    Comment actions Permalink
  • Marco Pirondini

    Well, your link is a very interesting git, because that described how an asynchronous detection takes place by queueing a frame and only processing its results when the next frame is available!

     

    Sencond thing I just tryed face-detection-adas-0001.xml and .bin as you suggested but also that model detect only the faces, when my research is to found an OpenVINO model dedicated exclusively to the detector of the head of a human subject seen from behind! Head in backside view to integrate it with a face detector to not loose detection ever if human subject go ahead, or go backward or simply turn head, without looking into the lens!

    Thank you

     

    0
    Comment actions Permalink
  • MartyG

    OpenVINO also has a head pose estimation model called head-pose-estimation-adas-0001 though does not specify whether the rear of the head is detectable. 

    https://docs.openvino.ai/2021.3/omz_models_model_head_pose_estimation_adas_0001.html

    0
    Comment actions Permalink
  • Marco Pirondini

    It is structured with 3 different detector models

    - OpenVino face-detection-retail-0005

    - OpenVino person-detection-retail-0013

    - and finally Tensorflow.compct.v1 HEAD_DETECTION_300x300_ssd_mobilenetv2.pb

    After a while a solved my issue whit MartyG similar suggest:

    Now the project is structured with new 3 different detector models (order are changed)

    - OpenVino human-pose-estimation-0001 (instead HEAD_DETECTION_300x300_ssd_mobilenetv2.pb)

    - OpenVino person-detection-retail-0013 (and/or person-detection-0200) '0200' is better to a close person

    - OpenVino face-detection-adas-0001 (instead face-detection-retail-0005) '0001' is better to a far face

    The first one works both far and close, but it has two 'problems' to do resolve:

    First problem it is asincrounous -) when it resolve its last frame queue, then I can apply the two last models in list. (the two last models are indented methods, but they works).

    Second problem the first model needed a parser that identify the head - ) with a simple but complete algoritm we can do it.

    I try to write to you a python code for this algoritm to detect Head from 'human-pose-estimation-0001':

    if hpe_pipeline.is_ready():
    frame = cv2.resize(image,(456, 256))
    ratio = (image.shape[1] / 456, image.shape[0] / 256)
      # Submit for inference
      hpe_pipeline.submit_data(frame, next_frame_id, {'img': image, 'ratio_frame': ratio})
                                        
      next_frame_id += 1
         
    else:
      # Wait for empty request
      hpe_pipeline.await_any()
                                    
    if hpe_pipeline.callback_exceptions:
      raise hpe_pipeline.callback_exceptions[0]

    results = hpe_pipeline.get_result(next_frame_id_to_show)
    if results:
      threshold = 0.1
    next_frame_id_to_show += 1
    (poses, scores), frame_meta = results
       img = frame_meta['img']
       ratio_frame = frame_meta['ratio_frame']

        if poses.size > 0:
            for pose in poses:
                points = pose[:, :2].astype(np.int32)
                #points = output_transform.scale(points)
                points_scores = pose[:, 2]
                # Draw joints.
                poses = np.zeros((19, 2), np.int32)
                
                
                for i, (p, v) in enumerate(zip(points, points_scores)):
                    if v > threshold:
                        #cv2.circle(img, tuple(p), 1, colors[i], 2)
                        #cv2.putText(img, str(i), tuple(p), cv2.FONT_HERSHEY_PLAIN, 1, (255,255,255), 1, cv2.LINE_AA) 
                      poses[i,0] = tuple(p)[0] * ratio_frame[0]
                        poses[i,1] = tuple(p)[1] * ratio_frame[1]
                        
                trovato = False

                if ((trovato == False) and
                    (poses[3,0] != 0 and poses[3,1] != 0) and
                    (poses[4,0] != 0 and poses[4,1] != 0)):
                    centerX = min(poses[3,0], poses[4,0]) + int(abs(poses[3,0] - poses[4,0])/2)
                    centerY = min(poses[3,1], poses[4,1]) + int(abs(poses[3,1] - poses[4,1])/2)
                    radius = int(abs(poses[3,0] - poses[4,0])/2)
                    trovato = True
                    
                if ((trovato == False) and
                    (poses[3,0] != 0 and poses[3,1] != 0) and
                    (poses[2,0] != 0 and poses[2,1] != 0)):
                    centerX = min(poses[3,0], poses[2,0]) + int(abs(poses[3,0] - poses[2,0])/2)
                    centerY = min(poses[3,1], poses[2,1]) + int(abs(poses[3,1] - poses[2,1])/2)
                    radius = int(abs(poses[3,0] - poses[2,0])/2)
                    trovato = True
                    
                if ((trovato == False) and
                    (poses[4,0] != 0 and poses[4,1] != 0) and
                    (poses[1,0] != 0 and poses[1,1] != 0)):
                    centerX = min(poses[1,0], poses[4,0]) + int(abs(poses[1,0] - poses[4,0])/2)
                    centerY = min(poses[1,1], poses[4,1]) + int(abs(poses[1,1] - poses[4,1])/2)
                    radius = int(abs(poses[1,0] - poses[4,0])/2)
                    trovato = True          

                if ((trovato == False) and
                    (poses[3,0] != 0 and poses[3,1] != 0) and
                    (poses[5,0] != 0 and poses[5,1] != 0) and       
                    (poses[6,0] != 0 and poses[6,1] != 0)):
                    centerXs = min(poses[5,0], poses[6,0]) + int(abs(poses[5,0] - poses[6,0])/2)
                    centerX = min(centerXs, poses[3,0]) + int(abs(centerXs - poses[3,0])/2)
                    centerY = poses[3,1] 
                    radius = int(abs(poses[3,0] - centerXs)/2)
                    trovato = True

                if ((trovato == False) and
                    (poses[4,0] != 0 and poses[4,1] != 0) and
                    (poses[5,0] != 0 and poses[5,1] != 0) and       
                    (poses[6,0] != 0 and poses[6,1] != 0)):
                    centerXs = min(poses[5,0], poses[6,0]) + int(abs(poses[5,0] - poses[6,0])/2)
                    centerX = min(centerXs, poses[4,0]) + int(abs(centerXs - poses[4,0])/2)     
                    centerY = poses[4,1] 
                    radius = int(abs(centerXs - poses[4,0])/2)
                    trovato = True
                    
                if ((trovato == False) and
                    (poses[3,0] != 0 and poses[3,1] != 0) and
                  (poses[0,0] != 0 and poses[0,1] != 0)):
                    centerX = min(poses[0,0], poses[3,0]) + int(abs(poses[0,0] - poses[3,0])/2)
                    centerY = min(poses[0,1], poses[3,1]) + int(abs(poses[0,1] - poses[3,1])/2)        
                    radius = int(abs(poses[0,0] - poses[3,0])/2)        
                    trovato = True
                    
                if ((trovato == False) and
                    (poses[0,0] != 0 and poses[0,1] != 0) and
                  (poses[4,0] != 0 and poses[4,1] != 0)):
                    centerX = min(poses[0,0], poses[4,0]) + int(abs(poses[0,0] - poses[4,0])/2)
                    centerY = min(poses[0,1], poses[4,1]) + int(abs(poses[0,1] - poses[4,1])/2)        
                    radius = int(abs(poses[0,0] - poses[4,0])/2)
                    trovato = True  
                    
                if ((trovato == False) and
                    (poses[4,0] != 0 and poses[4,1] != 0) and
                    (poses[2,0] != 0 and poses[2,1] != 0)):
                    centerX = min(poses[4,0], poses[2,0]) + int(abs(poses[4,0] - poses[2,0])/2)
                    centerY = min(poses[4,1], poses[2,1]) + int(abs(poses[4,1] - poses[2,1])/2)
                    radius = int(abs(poses[4,0] - poses[2,0])/2)
                    trovato = True
                    
                if ((trovato == False) and
                    (poses[3,0] != 0 and poses[3,1] != 0) and
                    (poses[1,0] != 0 and poses[1,1] != 0)):
                    centerX = min(poses[1,0], poses[3,0]) + int(abs(poses[1,0] - poses[3,0])/2)
                    centerY = min(poses[1,1], poses[3,1]) + int(abs(poses[1,1] - poses[3,1])/2)
                    radius = int(abs(poses[1,0] - poses[3,0])/2)
                    trovato = True   
                    
                if ((trovato == False) and
                    (poses[3,0] != 0 and poses[3,1] != 0)):

                    centerX = 0
                    if (poses[5,0] != 0 and poses[5,1] != 0):
                        centerXs = min(poses[5,0], poses[3,0]) + int(abs(poses[5,0] - poses[3,0])/2)
                        centerX = poses[3,0] 
                        
                    elif (poses[6,0] != 0 and poses[6,1] != 0):
                        centerXs = min(poses[6,0], poses[3,0]) + int(abs(poses[6,0] - poses[3,0])/2)
                        centerX = poses[3,0] 
                        
                    if (centerX != 0):
                        centerY = poses[3,1] 
                        radius = int(abs(poses[3,0] - centerXs))
                        trovato = True

                if ((trovato == False) and
                    (poses[4,0] != 0 and poses[4,1] != 0)):
                    
                    centerX = 0
                    if (poses[5,0] != 0 and poses[5,1] != 0):
                        centerXs = min(poses[5,0], poses[4,0]) + int(abs(poses[5,0] - poses[4,0])/2)
                        centerX = poses[4,0] 
                        
                    elif (poses[6,0] != 0 and poses[6,1] != 0):
                        centerXs = min(poses[6,0], poses[4,0]) + int(abs(poses[6,0] - poses[4,0])/2)
                        centerX = poses[4,0] 
                        
                    if (centerX != 0):
                        centerY = poses[4,1] 
                        radius = int(abs(poses[4,0] - centerXs))
                        trovato = True  
                        
                if (trovato == True):         
                    if ((poses[5,0] != 0 and poses[5,1] != 0) and       
                        (poses[6,0] != 0 and poses[6,1] != 0)):
                        centerYs = min(poses[6,1], poses[5,1]) + int(abs(poses[6,1] - poses[5,1])/2)
                        radius2 = int(abs(centerYs - centerY)/2) 
                        if radius < radius2: radius = radius2 
                    elif ((poses[5,0] != 0 and poses[5,1] != 0)):
                        radius2 = int(abs(poses[5,1] - centerY)/2) 
                        if radius < radius2: radius = radius2 
                    elif ((poses[6,0] != 0 and poses[6,1] != 0)):
                        radius2 = int(abs(poses[6,1] - centerY)/2) 
                        if radius < radius2: radius = radius2 
                                            
                if (trovato == True): 
                  # Put stuff here when you want to find Head

                    x1 = centerX  
                  y1 = centerY  
                    x0 = x1 - radius 
                    y0 = y1 - int(radius * 1.3)
                    w0 = x1 + radius
                    h0 = y1 + int(radius * 1.3)
                        
                  cv2.rectangle(img, (x0,y0), (w0,h0), (0,0,255), 2)
    # OR better
                  cv2.ellipse(img, (x1,y1), (int((w0-x0)/2),int((h0-y0)/2)), 0, 0, 360, (0,255,0), 2)
         
    0
    Comment actions Permalink
  • MartyG

    Thanks so much Marco Pirondini for sharing your knowledge and your code with the RealSense community!

    0
    Comment actions Permalink

Please sign in to leave a comment.