MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Javier Recasens As the camera is pointing straight down, the orientation should not make a difference to performance. The main influence that the orientation is likely to have is how much of t...
-
The discontinuance was part of a range of retirements for RealSense cameras not belonging to the 400 Series and also Intel-published first party RealSense software products listed at the link below...
-
Version 2.3.2 of the RealSense ROS1 wrapper is not too low as there were no more versions of that wrapper published after 2.3.2. Only the ROS2 wrapper continues to be updated now. And the 2.50.0 ...
-
Hi Julien Hyra It would depend on how large the lock of hair is. A single hair would be too thin for the camera to depth-sense. An object should be at least as large as a group of 9 pixels on th...
-
Hi Jeevaatre The official data sheet document for the D457 camera model lists its weight at approximately 145 grams on page 25 of the data sheet. For comparison, I placed a D457 on a real-wo...
-
If opencv_viewer_example.py works normally then this indicates that the camera and the USB connection are fine and the issue is with some aspect of your intel_camera_test.py script. What happens ...
-
Hi Jsyoon I checked your settings with a D435i in the RealSense Viewer tool, because if an FPS speed is chosen that is not supported by that resolution then the resolution automatically changes to...
-
I tested a D405 at 4 cm with a high Disparity Shift value of 200. The distance readout was incorrectly 0 at that distance. I found though that a good distance reading could be obtained if the Dep...
-
I located the case that was using a set of diodes. https://github.com/IntelRealSense/librealsense/issues/10429#issuecomment-1107853739 The D405 model is not equipped with an IMU component for tr...
-
The D435f model is fitted with a CLAREX NIR-75N filter on its sensors that absorbs visible light whilst permitting near-infrared light to pass through it. This IR pass filter enhances depth noise ...