MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Sub-millimeter refers to how the D405 has a minimum object detection accuracy at 7 cm distance that is as low as 500 microns (0.5 millimeters, hence 'sub-millimeter').
-
Hi Vittorio Lumare The mode switch is under a small removable cap on top of the D457 camera. There is not a screw to remove but a thin long object such as a sewing pin or a bent paperclip will ne...
-
You are very welcome. I'm pleased to hear that you were successful :)
-
Hi Kvuong The RealSense D405 camera is the only model that is officially described as having sub-millimeter accuracy. https://store.intelrealsense.com/buy-intel-realsense-depth-camera-d405.html ...
-
There was a recent case at the link below regarding an error caused by bag file playback in the 2.54.1 Viewer of bag files that were recorded in an earlier Viewer version (2.53.1 in that particular...
-
Use of the Python networking components 'pyrealsense2_net' and 'net_viewer.py' has a pattern of problems in past cases. If using 'from pyrealsense2' did not work then it is likely that pyrealsense...
-
You can export a single frame as a ply from the 3D point cloud mode of the RealSense Viewer tool using the 'Export' option at the top of the Viewer window when in 3D mode. You can view a bag file...
-
The link below has another case where this problem with pyrealsense2_net occurred. https://github.com/IntelRealSense/librealsense/issues/9946 The RealSense user in that particular case solved it ...
-
Aside from LIPScan 3D and rs-kinfu, most RealSense-compatible 3D scanning solutions are suited to large scenes rather than small objects on a turntable. The only remaining solution that would sui...
-
The ITSeez3D trial version's information on the ItSeez3D website indicates that it should support export for $7 per export. The RealSense SDK has an example program called rs-kinfu that can cr...