RealSense Support

D435i Raspberry Pi network transmission

Comments

7 comments

  • MartyG

    The RealSense SDK has a networking tool described at the link below that can be used with Raspberry Pi.  It is primarily designed for ethernet cabling but can be adapted for wi-fi communication.

    https://dev.intelrealsense.com/docs/open-source-ethernet-networking-for-intel-realsense-depth-cameras

     

    The tool was removed in SDK version 2.54.1 as it is planned that a new networking system will be replacing it in the next SDK version after 2.54.1.  So an SDK version earlier than 2.54, such as 2.53.1, will need to be used if you wish to experiment with the tool.

     

    Data sent from the Pi / camera to a central host computer can be accessed on the host through the RealSense Viewer tool or with program scripting.

    0
    Comment actions Permalink
  • 815613232

    thank you for your offer
    This solution is viewed through realsense viewer
    Is it possible to receive images through python application programming?

    0
    Comment actions Permalink
  • MartyG

    There is an example Python program called net-viewer for this networking tool below.

     

    *******************

     

    ## License: Apache 2.0. See LICENSE file in root directory.
    ## Copyright(c) 2021 Intel Corporation. All Rights Reserved.

    ###############################################
    ##      Network viewer                       ##
    ###############################################

    import sys
    import numpy as np
    import cv2
    import pyrealsense2 as rs
    import pyrealsense2_net as rsnet


    if len(sys.argv) == 1:
        print( 'syntax: python net_viewer <server-ip-address>' )
        sys.exit(1)

    ip = sys.argv[1]

    ctx = rs.context()
    print ('Connecting to ' + ip)
    dev = rsnet.net_device(ip)
    print ('Connected')
    print ('Using device 0,', dev.get_info(rs.camera_info.name), ' Serial number: ', dev.get_info(rs.camera_info.serial_number))
    dev.add_to(ctx)
    pipeline = rs.pipeline(ctx)


    # Start streaming
    print ('Start streaming, press ESC to quit...')
    pipeline.start()

    try:
        while True:

            # Wait for a coherent pair of frames: depth and color
            frames = pipeline.wait_for_frames()
            depth_frame = frames.get_depth_frame()
            color_frame = frames.get_color_frame()
            if not depth_frame or not color_frame:
                continue

            # Convert images to numpy arrays
            depth_image = np.asanyarray(depth_frame.get_data())
            color_image = np.asanyarray(color_frame.get_data())

            # Apply colormap on depth image (image must be converted to 8-bit per pixel first)
            depth_colormap = cv2.applyColorMap(cv2.convertScaleAbs(depth_image, alpha=0.03), cv2.COLORMAP_JET)

            depth_colormap_dim = depth_colormap.shape
            color_colormap_dim = color_image.shape

            # If depth and color resolutions are different, resize color image to match depth image for display
            if depth_colormap_dim != color_colormap_dim:
                resized_color_image = cv2.resize(color_image, dsize=(depth_colormap_dim[1], depth_colormap_dim[0]), interpolation=cv2.INTER_AREA)
                images = np.hstack((resized_color_image, depth_colormap))
            else:
                images = np.hstack((color_image, depth_colormap))

            # Show images
            cv2.namedWindow('RealSense', cv2.WINDOW_AUTOSIZE)
            cv2.imshow('RealSense', images)
            k = cv2.waitKey(1) & 0xFF
            if k == 27:    # Escape
                cv2.destroyAllWindows()
                break

    finally:
        # Stop streaming
        pipeline.stop()

    print ("Finished")
    0
    Comment actions Permalink
  • 815613232

    Thanks for your guidance
    I deployed according to the plan. I successfully compiled the SDK 2.53 version on the Raspberry Pi. By running the rs-server tool, I successfully received the screen through realsense-viewer on my PC.
    I now successfully compile SDK 2.53 on another PC (ubuntu system) and generate the following .o .so file

     

     

    But I am getting an error like below when running the py code you provided

    The error shows that there is no library for pyrealsense_net, but I have successfully compiled this library file. Why is this? Can you provide a solution?

    0
    Comment actions Permalink
  • MartyG

    The link below has another case where this problem with pyrealsense2_net occurred.

    https://github.com/IntelRealSense/librealsense/issues/9946

     

    The RealSense user in that particular case solved it by replacing import pyrealsense2_net as rsnet with the instruction below.

    from pyrealsense2 import pyrealsense2_net as rsnet
    0
    Comment actions Permalink
  • 815613232

    I followed your tips and used from pyrealsense2 import pyrealsense2_net as rsnet
    But an error is reported, as follows

    0
    Comment actions Permalink
  • MartyG

    Use of the Python networking components 'pyrealsense2_net' and 'net_viewer.py' has a pattern of problems in past cases.  If using 'from pyrealsense2' did not work then it is likely that pyrealsense2_net is not going to work for you, unfortunately, and it will not be fixed as development of this networking tool has ceased.

     

    There is an alternative RealSense networking tool for Python called EtherSense but it has not been tested with a wireless connection.

    https://github.com/krejov100/EtherSense

    https://dev.intelrealsense.com/docs/depth-camera-over-ethernet-whitepaper

    0
    Comment actions Permalink

Please sign in to leave a comment.