MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
I believe that the updated script was libuvc_installation.sh which is part of the libuvc backend method of installing librealsense. This method is recommended for Arm-based devices such as the Pi....
-
Expand open the Coded Light Depth Sensor options and left-click on the boxes beside the Depth and the Infrared 1 options. You can toggle the boxes between blue color (on) and black color (off). T...
-
The situation that you describe sounds straightforward to implement. Yes, the SR300 can display a live infrared stream. In regard to recording, you have a couple of options. - Use the RealSense ...
-
If you are using the camera outdoors then I recommend enabling the camera's auto-exposure in your script. This will enable the camera to automatically adjust to changing outdoor light conditions. ...
-
I wouldn't say it was related to stereo depth particularly but rather the time that it takes for auto-exposure to adjust to the environmental conditions when the stream activates. So I would recom...
-
Cubemos seems to treat joints individually. Parts that cannot be calculated disappear whilst the rest of the joints remain, and invisible joints instantly reappear as soon as they can be calculate...
-
Hi Matan Traditionally, performing skeletal detection on people in unusual poses such as laying down, or when "off screen" from the camera's view, has always been difficult. Microsoft's Kinect 1 ...
-
The old 2016 documentation used to have individual versions for particular SDK versions, but the current SDK's documentation does not. The same documentation gets updated over time. So yes, the a...
-
Stereo Depth cameras do not interfere with other Stereo Depth cameras of the 400 Series type, but my recollection is that they interfere with coded light. Coded light would interfere with coded lig...
-
Hi Amitelle1337 Yes, coded light cameras such as the RealSense SR300 / SR305 will interfere with each other. Microsoft's research labs once tested a "shake n sense" system for disrupting coded-lig...