MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Zahid Iqbal When aligning depth to color with the align_to instruction, the center-line of the color sensor becomes the 0, 0, 0 origin of depth. When depth and color are not aligned, the 0,0,0...
-
Hi Matan RealSense 400 Series cameras can make use of any visible or near-IR light sources in ranges between 400 and 1000 nm. If your UVC light's peak wavelength is 254 nm though then it is likel...
-
Hi Nrodrigues If you have access to the RealSense Viewer tool, please try resetting the camera with the incorrect distance value to its factory-new default calibration using the instructions at th...
-
Hello, is your Arm computer an Nvidia Jetson board? At the link below, there is a past report of a chromatic aberration when comparing Ubuntu on a Jetson Nano computing board with Arm architecture...
-
Hi Jack Jansen The profile.get_stresm instruction may provide what you need. Below are links to references for C++ and Python. C++ https://github.com/IntelRealSense/librealsense/issues/2693 a...
-
Hi Info As long as the window placed in front of the camera is completely clear and does not have any properties that filter or distort the light passing through it then the filtering on the D455f...
-
If the distance between cameras is less than 3 meters then the simple sync cable design in the image below is suggested, used with cables that are of the shielded twisted pair type. This should pr...
-
The approach that Intel took to this capture process in a February 2018 demo at the Sundance Festival was to put each of four RealSense cameras on a separate PC like you did and hardware sync them,...
-
Would it be possible to take a film studio approach with the recording and do two 'takes' of the scene with the actors so that you have back-up recordings, and check playback after each take to con...
-
Hi Jack Jansen Yes, it is recommended that the master camera is started first. Use of hardware sync is not always necessary for multiple camera projects, and this sounds like a project that woul...