RealSense Support

Effect of UVC light on camera preformace

Comments

1 comment

  • MartyG

    Hi Matan  RealSense 400 Series cameras can make use of any visible or near-IR light sources in ranges between 400 and 1000 nm.  If your UVC light's peak wavelength is 254 nm though then it is likely that the camera will not see it and so will not be affected by it.

     

    Just in case though, you could further minimize the risk of interference by setting a camera option called Power Line Frequency to '60' to match the frequency of lights that operate in the 60 Hz range.

    0
    Comment actions Permalink

Please sign in to leave a comment.