MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Sohwa427 Thanks very much for your questions. 1. RealSense 400 Series stereo cameras do not use RGB to generate depth data. The camera has a left and right infrared sensor (hence the term '...
-
You can increase the strength of the infrared dot projection by increasing the Laser Power setting from its default value of '156' to its maximum of '360'. This makes the pattern more visible to t...
-
Can you confirm whether you are using C++ or C# language please?
-
Hello, the missing depth data on the table area that the plant is resting in is likely because the table is dark gray / black in color. This is because it is a general physics principle (not speci...
-
Hi Janeelona2350576 Are you able to receive frames if you place wait_for_frames() inside a try: while True streaming loop like in the pyrealsense2 wrapper's example test program at the link below,...
-
Hi D Vandegraaf5 Most RealSense 400 Series stereo depth camera models except D405 can operate in the dark as they are equipped with an infrared projector component. The 400 Series cameras also pe...
-
Hi Pink Spear I researched all the cases I could find on the internet regarding this particular error, which I have not seen before. Of all the cases, the only one with a suggested solution advis...
-
Hi Yoshiya Yamaue This error may occur if you are trying to save a bag file to a folder location on the computer that does not have write permission. You can set a path to save the bag file to in...
-
Hi Jimmek M4 (4 mm diameter) is the size of the two small mounting holes on the back of the camera on the D455 camera model. D415 and D435 / D435i type cameras have an M3 size mounting hole diamet...
-
When a hardware reset is performed, the camera disconnects at around the 30% point in the process and then reconnects. The DS5 group_devices is empty message that you experienced during hardware r...