MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Dmitrii Sokolov The link below lists nm frequencies for each product (W, R, B, G) in the LTPRHP3W range. https://machinevisionstore.com/catalog/details/1453 The model with a blue LED is 460 n...
-
Hello! I would first recommend updating your RealSense SDK and camera firmware to the latest versions if possible. SDK 2.15.0 is from August 2018 and the camera firmware version is extremely old ...
-
You are very welcome. Yes, that is correct. The dot pattern adds readable texture source to the surface of flat objects that lack texture.
-
The link below is Intel's own librealsense guide to Raspbian installation on a Pi 3. It may be adaptable for Pi 4. https://github.com/IntelRealSense/librealsense/blob/master/doc/installation_raspb...
-
https://dev.intelrealsense.com/docs/stereo-depth-camera-d400#cad-files
-
Hello, the D435 camera model has a smaller field of view size on its RGB sensor than the depth sensor. So when using the get_distance() instruction, the ideal approach is to (1) perform depth to c...
-
Hi Harinixp Please try an RGBD launch instead to generate a pointcloud by following the steps below. 1. Input the instruction below to install support for an RGBD launch on Noetic. sudo apt-ge...
-
Hi Kanakshilledar111 The error Failed to read busnum/devnum is a very rare one. In the past it has usually occurred when using RealSense cameras with low-power computing boards that have been una...
-
The IR-Cut filter is listed as part of the infrared sensor component on the D405's camera circuit board, indicating that it is not likely to be removable without damaging the sensor. I know of...
-
Hi Rohan A I have recommended the use of a visible pattern projector with the D405 camera model (see the link below), as this camera model cannot see invisible infrared projections due to being eq...