RealSense Support

The distance to the object is not correctly determined if the object is not on the same axis as the camera

Comments

12 comments

  • MartyG

    Hello, the D435 camera model has a smaller field of view size on its RGB sensor than the depth sensor.  So when using the get_distance() instruction, the ideal approach is to (1) perform depth to color alignment in order to map depth and color data together, and (2) use color intrinsics, because after depth-color alignment the origin point of depth changes from the center of the left IR sensor to the center of the RGB sensor.

     

    If depth and color are not aligned and color intrinsics are not used then measurements may be accurate at the center of the image but become increasingly inaccurate when checking coordinates towards the edges of the image.

     

    A Python script at the link below that uses alignment and color intrinsics may be a helpful reference.

    https://support.intelrealsense.com/hc/en-us/community/posts/23541262437011/comments/23566066750355

    1
    Comment actions Permalink
  • 7159486

    I'm sorry, this link doesn't work

    0
    Comment actions Permalink
  • MartyG

    The link works if you copy it and paste it into the browser address window instead of clicking on the link.  I will put the script here though so that you do not need the link.

     

    import pyrealsense2 as rs
    import numpy as np
    import math
    import cv2

    pipeline = rs.pipeline()
    config = rs.config()
    config.enable_stream(rs.stream.depth, 640, 480, rs.format.z16, 30)
    config.enable_stream(rs.stream.color, 640, 480, rs.format.bgr8, 30)
    pipeline.start(config)

    align_to = rs.stream.depth
    align = rs.align(align_to)

    target_x = 320
    target_y = 240

    try:
        while True:
            # This call waits until a new coherent set of frames is available on a device
            frames = pipeline.wait_for_frames()

            # Aligning color frame to depth frame
            aligned_frames = align.process(frames)
            depth_frame = aligned_frames.get_depth_frame()
            aligned_color_frame = aligned_frames.get_color_frame()

            if not depth_frame or not aligned_color_frame:
                continue

            color_intrin = aligned_color_frame.profile.as_video_stream_profile().intrinsics

            # Draw two perpendicular lines
            cv2.line(color_image, (target_x, 0), (target_x, 480), (0, 0, 255), 2)  # Vertical line
            cv2.line(color_image, (0, target_y), (640, target_y), (0, 0, 255), 2)  # Horizontal line

            # Display the image with the changes
            cv2.imshow("Color Image", color_image)

            # Blur the image to reduce noise
            blurred_image = cv2.GaussianBlur(color_image, (25, 25), 0)

            # Convert the image to grayscale for better processing performance
            gray_image = cv2.cvtColor(blurred_image, cv2.COLOR_BGR2GRAY)

            # Find circles in the image
            circles = cv2.HoughCircles(
                gray_image,
                cv2.HOUGH_GRADIENT,
                dp=1,
                minDist=20,
                param1=50,
                param2=30,
                minRadius=0,
                maxRadius=0
            )

            if circles is not None:
                circles = np.uint16(np.around(circles))

                for circle in circles[0, :]:
                    # Get the coordinates of the circle's center and its radius
                    x, y, radius = circle

                    depth_width = depth_frame.get_width()
                    depth_height = depth_frame.get_height()

                    if 0 <= x < depth_width and 0 <= y < depth_height:
                        depth_at_center = depth_frame.get_distance(x, y)
                        depth_at_center_cm = depth_at_center * 100  # Convert to centimeters

                        # Continue processing depth data
                    else:
                        print("Coordinates (x, y) are outside the valid range of the depth image.")

                    # Display depth on the color image
                    depth_text = "     {:.2f} cm".format(depth_at_center_cm)
                    cv2.putText(color_image, depth_text, (x, y), cv2.FONT_HERSHEY_SIMPLEX, 0.5, (0, 0, 255), 2)

                    # Depth at the center of the circle
                    depth_value = depth_at_center_cm  # Replace with the depth at the center of the circle

                    # Calculate 3D coordinates
                    dx, dy, dz = rs.rs2_deproject_pixel_to_point(color_intrin, [x, y], depth_value)

                    distance = math.sqrt(((dx) ** 2) + ((dy) ** 2) + ((dz) ** 2))

                    # Print the manually calculated 3D coordinates of the circle center
                    print("Manually calculated 3D coordinates of the circle center (X, Y, Z):", (dx, dy, dz))

                    # Draw the circle and center on the color image
                    cv2.circle(color_image, (x, y), radius, (0, 255, 0), 2)
                    cv2.circle(color_image, (x, y), 2, (0, 0, 255), 3)

                    # Display the resulting image
                    cv2.imshow('Detected Circles with Depth', color_image)

            # Wait for the 'q' key to exit the loop
            if cv2.waitKey(1) & 0xFF == ord('q'):
                break

    finally:
        # Close the connection and clean up
        pipeline.stop()
        cv2.destroyAllWindows()
    0
    Comment actions Permalink
  • 7159486

    Thanks so much for the reply! Can you tell me why I have to write so much code to get the distance to a point? Isn't this implemented in the RealSense library itself as a single method? Or maybe there is a library in which it is implemented?

    0
    Comment actions Permalink
  • MartyG

    A simpler method would be to use only the depth data and not the RGB to get the distance in meters.

     

    import pyrealsense2 as rs
    import numpy as np

    pipeline = rs.pipeline()

    # Start streaming
    pipeline.start()

    frames = pipeline.wait_for_frames()
    depth = frames.get_depth_frame()

    width = depth.get_width()
    height = depth.get_height()

    dist = depth.get_distance(width/2, height/2)
    print(dist)

    # Stop streaming
    pipeline.stop()

     

    In the line dist = depth.get_distance(width/2, height/2), dividing the width and height values of the depth resolution by half gives the center coordinate of the image.  For example for 1280x720 depth resolution, 1280 / 2 and 720 / 2 gives the center coordinate 640, 360 for the image. 

    0
    Comment actions Permalink
  • 7159486

    Thank you. That's the code we originally sent in this request. What is the difference between what you sent and the code in the first message? This code doesn't work.

    0
    Comment actions Permalink
  • MartyG

    The most obvious difference is that the script above is using the resolution width and height values directly from the frame information, whilst your original script at the beginning of this case stores stream values in numpy (np) arrays.  The arrays do not seem to be used for anything in the script though as the depth value used in get_distance is still being retrieved directly from the pipeline via depth_frame

    depth_frame.get_distance(x, y) * 1000
    0
    Comment actions Permalink
  • 7159486

    The thing is, I don't get the distance from depth_image, which is in the form of (np) arrays, I also get it from depth_frame = frames.get_depth_frame()

    I attach a picture of the code that is used 

    0
    Comment actions Permalink
  • MartyG

    Multiplying depth.get_distance(x, y) by 1000 is not usually done.  Doing so may be combining together two different methods of obtaining the distance that should not be used together.  The alternative approach to using get_distance is to retrieve the raw depth value of the distance and then multiply it by 0.001 meters / 1000 mm to get the distance in real-world meters.  The value output by get_distance() does not need to be converted to meters as it is already expressed in meters. 

     

    How do the measurements behave if you remove the multiplication, please?

     

    depth = depth.get_distance(x, y)

     

     

    0
    Comment actions Permalink
  • 7159486

    We've tried everything, but still your example gives a distance of 0 everywhere except the center

    0
    Comment actions Permalink
  • 7159486

    and on the large resolution even in the center does not give the distance

    0
    Comment actions Permalink
  • MartyG

    Do you get results if you test the Python script at the link below, which instead of get_distance uses the method of multiplying the raw pixel depth value by the depth scale?

    https://github.com/IntelRealSense/librealsense/issues/3473#issuecomment-474637827

    0
    Comment actions Permalink

Please sign in to leave a comment.