Jake Min
- Total activity 7
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Comments
Recent activity by Jake Min-
My solution was to reconnect F455 to Android and remove the device again. Removed after applying UNPAIR in the RealSenseID app menu.
-
Revathi, I've had this problem before. I also used it on Windows 10, but sometimes I tested the F455 on an Android device as well. The cause of the problem is that when removing F455 from an Androi...
-
If a problem occurs while the tool is looking for the firmware: The cause is not a corrupt or installation error in the download package. The result was the same with a fresh download or reinstall....
-
Currently, SDK v2.41.0 and new firmware are only available for L515 users. Since the separate firmware image has not yet been updated, you should try the update through the Recommended Updates pop-...