RealSense Support

Intel Realsense ID f455 sdk does not work in my windows 10 system

Comments

6 comments

  • Jesus Garcia

    Hello Revathi,

    Did the rsid-viewer work before? If so, what changed?

    Do the other sample programs work?

    I saw you opened another request because of problems with rsid-cli.exe.

    Sincerely,
    Jesus G.
    Intel Customer Support

     

    0
    Comment actions Permalink
  • Jesus Garcia

    Revathi,

    Also, describe how the RealSenseID is connected to the host system. 

    Is the RealSense ID connected directly to a PC via the USB port?

    0
    Comment actions Permalink
  • Jake Min

    Revathi,

    I've had this problem before.

    I also used it on Windows 10, but sometimes I tested the F455 on an Android device as well.

    The cause of the problem is that when removing F455 from an Android device, you must apply UNPAIR from the menu and then remove it.

    Otherwise, you will experience Query Error and Authenticator Error when connecting to a new device.

    0
    Comment actions Permalink
  • Jake Min

    My solution was to reconnect F455 to Android and remove the device again.

    Removed after applying UNPAIR in the RealSenseID app menu.

    0
    Comment actions Permalink
  • Revathi

    Hi jakemin,

    I am also having the same issue and now it's resolved. Thanks for your solution.

    1
    Comment actions Permalink
  • Rahul R

    But i Didn't connect with android. I connected to cpu. 

    Can you give me solution for this becouse it was working fine earlier with linux as well window .

    0
    Comment actions Permalink

Please sign in to leave a comment.