Dmitrii Sokolov
- Total activity 16
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 4
Posts
Recent activity by Dmitrii Sokolov-
Precise measuring the object volume (Spatial resolution issue)
Hello everybody, hello MartyX Grover I am implementing depth cameras to precisely measure volume of objects placed on a table parallel to the camera (so the camera looks vertically from above). Giv...
-
Software trigger / single image D405
Is it possible to capture a single image on a D405 via a software command? I mean, not grab an image from the stream, but rather trigger the capture of a single frame programmatically? Preferably i...
-
Depth accuracy for a particular application
Hello MartyG, hello everyone, this time I'd like to ask how could I estimate or measure the accuracy for a particular application? Camera: D405 First, let's consider ideal conditions. In different ...
-
D405 and a Projector
Hello everybody, I am interested in combining a D405 (or two of them) with a projector to enhance depth recognition quality when scanning concrete surfaces, which are relatively homogeneous. I have...