Zahid Iqbal

  • Total activity 45
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 9

Posts

Recent activity by Zahid Iqbal Recent activity Votes
  • D455 depth camera point cloud

    MartyG I am using realsense D455 camera. My question is when we want to save a point cloud, is it only based on the depth data, i.e., the stream that is enabled via depth sensor? Imagine that as a ...

  • orientation of a point in the camera coordinate system

    MartyX Grover We have approaches that return 3d point in the camera reference frame, given a 2d pixel point. Is there any method, or approach that can given us the rotation / orientation of a point...

  • D455 the coordinate system

    MartyX Grover Looking at the D455 camera model from the front, the order from left to right is: Right Infrared sensor, RGB sensor, Infrared Projector and Left Infrared sensor. I want to understand...

  • D455 camera matrix

    MartyG I am using D455 camera, and I need its camera matrix and distortion coefficients for a camera pose estimation algorithm. I started realsense-viewer, and tried the following. on-chip calibrat...

  • efficient way to retrieve 3d mapping for several 2d pixel points

    MartyG I have several points that I want to retrieve 3d mapping. I have a bounding box of some object(s) in the scene. I am listing all the pixel points that lie within this bounding box. My idea i...

  • coordinate mapping issue between data captured in separate functions

    MartyG Following on some previous discussions regarding mapping between 2D pixel points and 3D coordinates, I have some points that I'd like to make.  Of the three methods suggested for calculating...

  • D455 the coordinate frames

    MartyG I have tested the functions to find 3D position of a given pixel point using methods suggested in other post. My question is what is the origin of the coordinate frame here, and it is locate...

  • finding 3d coordinates of a given point which is specified in the 2d pixel coordinates

    Hi, My question is regarding finding 3d coordinates of a given point which is specified in the 2d pixel coordinates. I have read some similar threads on the above issue. In the realsense-viewer, wh...

  • some information needed about D455

    Hi, As a new person to the computer vision field, I recently started using the "intel realsense 455" camera. I can see, there appear to be 4 sensors on the camera. I understand, one of these is to ...