RealSense Support

D455 depth camera point cloud

Comments

1 comment

  • MartyG

    Hi Zahid Iqbal  If you only need to generate a single frame of point cloud then you could export depth, or depth and color, to a .ply format pointcloud data file.  That .ply could then be imported into a 3D modelling program such as MeshLab or Blender for further editing and conversion into a solid mesh object if you wish to do so. 

     

    A guide to doing so with the RealSense Viewer tool and the open-source software MeshLab is at the link below.

    https://www.andreasjakl.com/capturing-3d-point-cloud-intel-realsense-converting-mesh-meshlab/

     

    If you wish to create your own script to export a pointcloud to .ply file then both C++ and Python languages can do so.  However, for a .ply that contains color information, C++ will be the best language to use as Python has problems with exporting color pointcloud data to a .ply.

     

    If the saved pointcloud has to be a continuous stream instead of a single frame then you could record both depth and color streams to a bag file and then use that file as the 'data source' instead of a live camera to generate a point cloud from the file's stored streams as though a live camera was being used.

     

    The minimum height of the mount will be dictated by the minimum depth sensing range of the camera.  For the D455 camera model, the camera should be positioned at least 0.5 meters from the object.

    0
    Comment actions Permalink

Please sign in to leave a comment.