Chozo
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by Chozo-
Unfortunately this did not work either, it is not detected. Other SR300 cameras are detected fine but this one which has been bricked is not detected at all.
-
Unfortunately that doesn't work either. The driver was reinstalled and it still has the same issue. There was no crashing involved in any form. This is occurring on several different systems with t...
-
For report comparison, this is the same issue occurring on another internet connected unit which too has the DCM+SDK installed and has previously used a working SR300. This too shows the same issue...
-
Yes, this machine has internet and the DCM/drivers as well as the SDK. They were previously installed on this very machine and are still installed. The cameras section does not show because the cam...
-
I have tried that as well to no joy with my phone at 43%. It is the cameras own internal "Generic SuperSpeed USB Hub" reporting insufficient power not the PC or externally powered hub that it is co...
-
I have tried the newer DCM as well [3.4.104.3435] to only find it cannot be installed due to 'no realsense device detected'. It is the one I was using previously before trying the older version for...