Chozo

  • Total activity 8
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Chozo
  • Chozo commented,

    Unfortunately this did not work either, it is not detected. Other SR300 cameras are detected fine but this one which has been bricked is not detected at all.

  • Chozo commented,

    Unfortunately that doesn't work either. The driver was reinstalled and it still has the same issue. There was no crashing involved in any form. This is occurring on several different systems with t...

  • Chozo commented,

    For report comparison, this is the same issue occurring on another internet connected unit which too has the DCM+SDK installed and has previously used a working SR300. This too shows the same issue...

  • Chozo commented,

    Yes, this machine has internet and the DCM/drivers as well as the SDK. They were previously installed on this very machine and are still installed. The cameras section does not show because the cam...

  • Chozo commented,

    I have tried that as well to no joy with my phone at 43%. It is the cameras own internal "Generic SuperSpeed USB Hub" reporting insufficient power not the PC or externally powered hub that it is co...

  • Chozo commented,

    I have tried the newer DCM as well [3.4.104.3435] to only find it cannot be installed due to 'no realsense device detected'. It is the one I was using previously before trying the older version for...

  • Chozo created a post,

    RealSense SR300 bricked by older DCM Version.

    Greetings! Unsure where to start to further diagnose the issue. I've been using a Realsense SR300 flawlessly for over a year now under Windows 10. However, I came across some new software which exh...