7159486
- Total activity 22
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 4
Posts
Recent activity by 7159486-
What distance does the camera show
Hi! Can you tell me if the D435 camera measures the distance to the plane in which the object is located or directly to the object itself? The picture shows it. That is, the camera measures X dista...
-
The distance to the object is not correctly determined if the object is not on the same axis as the camera
This code, written in python for the D435 camera, works fine - you can fairly accurately determine the distance to an object that is in a straight line with the camera. But if the object moves side...
-
Cannot access the L515 camera using the python pyrealsense2 library on a Rasberry Pi4
Cannot access the L515 camera using the python pyrealsense2 library on a Rasberry Pi4. Segmentation Fault error occurs, which has its root in the depths of RealSense SDK 2.0, built from source. At ...