Bschwartz

  • Total activity 19
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 6

Posts

Recent activity by Bschwartz Recent activity Votes
  • D455 Partial Frames

    Seeing partial frames periodically running multiple D455s, all plugged into USB3 PCIe cards. What could be causing this issue? Link to video clip below. https://drive.google.com/file/d/1wqmuYhLwn4k...

  • Sync D455 array to Optitrack motion capture sensors

    Is it possible to sync an array of D455 cameras to an array of Optitrack motion capture sensors for parallel capture? The Optitrack has a box that allows for external sync: https://www.optitrack.co...

  • D455 -- Exposure time and motion blur

    Possibly a vague question, but has anyone determined the cutoff for D455 exposure time where it doesn't present noticeable motion blur when recording normal human action? I know the cameras don't h...

  • Sync timestamp of RealSense to different camera

    This question has been asked before, but I haven't seen a definitive or clear answer: how can I sync the timestamp of a RS to a non-Intel camera? I'm not referring to actual board-level sync or gen...

  • Various kinds of calibration

    What are the functional differences between on-chip self calibration, dynamic calibration, and OEM calibration?

  • Sync D455 array to 3rd party camera array

    Running a D455 camera array, using one camera as master and the others as slave to achieve sync. If I wanted to sync this camera array to a second camera array composed of 3rd party RGB-only camera...