Javier Recasens

  • Total activity 14
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 4

Posts

Recent activity by Javier Recasens Recent activity Votes
  • No Temperature enabled for D457 (Python)

    Im using a D457 camera but it looks like there is no support for any of the temperature readings when using pyrealsense2. HW Firmware: 5.15.0.2pyrealsense2 (2.54.1.5217) ...sensor = profile.get_dev...

  • Position of Camera for Moving Object Reconstruction

    Hello, I’m using a fixed D457 camera to capture the top section of a moving object for 3D reconstruction. I'm curious about the optimal camera positioning to improve triangulation in stereo matchin...

  • D457 - Waterproof USB-C connection

    Hello, I need assistance in protecting the USB-C connection of the D457 camera that I plan to use outdoors. The camera has an IP65 rating, which should protect it from dust and projected water. How...