Javier Recasens
- Total activity 14
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 4
Comments
Recent activity by Javier Recasens-
I was able to make it work. Device must be enabled and streaming. Example: https://github.com/IntelRealSense/librealsense/issues/866
-
What I find most strange is that the sensor does support some of the temperature options (such as <option.asic_temperature: 23> and <option.projector_temperature: 25>: sensor.get_supported_options(...
-
You could use an interval of quantiles (e.g. 5% to 95%) to set all pixel depth values outside that range to zero (or impute with the median or nearest neighbor).
-
As always, Thanks Marty. A side-on camera orientation (or camera being parallel to the object's movement direction) makes sense, I can use less frames for the reconstruction.
-
MartyG Could we get confirmation that the USB Type-C connector (Female Receptacle) of the D457 camera is waterproof? To ensure waterproof capabilities in the D457 camera, it is important to conside...
-
Thanks. I think the IP68 product I could use are: Amphenol LTW UC30ML-NCML-QB001 Bulgin PXP4040/C/A/1M00 I wonder if these are recommended cables... My concern is that they do not have "Screw Locki...