Michael Tandy
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Activity overview
Latest activity by Michael Tandy-
Michael Tandy commented,
rs2_config_enable_stream( config, RS2_STREAM_COLOR, 0, 960, 540, RS2_FORMAT_RGB8, 6, &e); check_rs_error(e); rs2_config_enable_stream( config, RS2_STREAM_DEPTH, 0, 320, 240,...
-
Michael Tandy created a post,
What are the details of firmware bug RS5-5453
Hello! I want to obtain a single colour image from each of several L515s, all of which are connected over the same USB connection. As the USB connection only has the bandwidth for one or two camera...
-
Michael Tandy created a post,
L515 Feature request: Software API to turn off IR
Hello! I would like to request a feature for the L515 - the ability to turn off the IR emitter through software. I'm aware I can use the "hardware sync pin" to enable and disable the IR emitter but...