What are the details of firmware bug RS5-5453
Hello!
I want to obtain a single colour image from each of several L515s, all of which are connected over the same USB connection. As the USB connection only has the bandwidth for one or two cameras to run at a time, I need to be able to start and stop colour video quickly.
The inter-cam sync mode is not a solution in this case, as it only controls depth data - not colour data.
Currently the SDK has a built in delay which means you cannot stream less than two seconds of colour video. The code says it's to work around a firmware bug, RS5-5453
Please can you provide some details about the bug? For example:
- What are the symptoms of the bug?
- Has the bug been fixed in more recent versions of the firmware?
Thanks very much!
-
Hello Michael,
Thank you for contacting us.
We suggest you open a thread on Github, where you'll directly associate with the developers.
Sincerely,
Zulkifli Halim
Intel Customer Support
Please sign in to leave a comment.
Comments
1 comment