Ahabeillon
- Total activity 16
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 4
Posts
Recent activity by Ahabeillon-
Windows Server 2019 issue
Hi, I try to use a D435 on a server using 'Windows Server 2019 Version 1809 (OS build 17763.2061)'.I'm using 'SDK-Win10-2.47.0.3309'.When I open 'RealSense Viewer' nothing apperas.But thanks 'Devi...
-
C# Rotated flux
Hi, a simple question, is it possible to obtain directly a rotated image flux thanks a setting? Thanks a lots,Regards
-
D455 C# AccessViolationException
Hi,I work with a colleague on a new application with lot of D455 cameras (between 8 to 16).Our problem is, after few minutes, an error appears in processedFrames. We don't understand why.Our projec...
-
C# D435 Histogram Equalization
Hi,I'm the owner of an IntelrealSense D435. I'm writing a code in C# to connect the camera without problem.Right now, i would like to 'Enable or Disable' the 'histogram equalization'. I have found ...