Yu-Chern Peh
- Total activity 217
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 86
Comments
Recent activity by Yu-Chern Peh-
Hi Laubarbara3, We want to thank you for your inquiry with regards to T265. We are familiar with known inconsistent tracking result that occur with T265. We have moved our focus to our next genera...
-
Hi Camnagg,There have been several discussions previously in RealSense Community and GitHub about this issue. It seems like copying the library files next to the script tends to solve the issue. Bu...
-
Hi Dkyun, This is the expected behavior that the IR illuminators will light up for every authenticate process. If you run the authenticate process in loop, then the IR illuminators will blink. It...
-
Hi Golovin, 1) L515 camera requires a USB-C 3.1 cable to connect to host machine to provide power and transfer data during operation. Since, the supply power of the device is provided by the comp...
-
Hi Jw1202 Lee, The HSF100 is a flexible interposer cable specifically designed for connecting Intel® RealSense™ modules to the Intel® D4 processor boards. They are available individually or in 8 ...
-
Hi Munther Basuni, Intel® RealSense™ Touchless Control Software supports a variety of kiosks and digital signs, ranging in size from 11 to 32 inches. You can mount the distance between camera and...
-
Hi Cloudtenno, Please make sure you are using the compatible firmware for the specific version of RealSenseID. For example: Use firmware, F450_4.3.0.8200_SKU1_SIGNED.bin for RealSenseID Versio...
-
Hi, L515 uses reflected light to calculate the distance of objects, hence any of the ambient or artificial lights may affect the performance of L515. However, we have control of the laser power a...
-
Hi Rakesh, Sorry for our late response. Is the issue still persists? Try to connect with different USB 3.0 cables. Regards, Yu-Chern Intel Customer Support
-
Hi Kaitei, For device mode, the user database information is saved inside the device. For host mode, the user database information is saved inside a db file. Regards, Yu-Chern Intel Custom...