View my account

Intel® RealSense™ Touchless Control Software Maximum screen size and distance?

Comments

1 comment

  • Yu-Chern Peh

    Hi Munther Basuni,

     

    Intel® RealSense™ Touchless Control Software supports a variety of kiosks and digital signs, ranging in size from 11 to 32 inches. You can mount the distance between camera and the top screen depending on the screen size, orientation and other factors. Hence, 40 inch screen should be no issue. 

     

    Intel® RealSense™ Touchless Control Software is designed with the concept of "from touch to touchless", which allow user to interact directly with screens or surfaces without physically touching them. I am sorry that I unable to provide you an exact maximum distance away from the screen as it may vary from mounting the camera with the top screen. However, the virtual touch plane which you desire a 80cm distance seems not possible because it is not designed for long-distance control. 

     

     

    Regards,

    Yu-Chern

    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.