Yu-Chern Peh
- Total activity 217
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 86
Comments
Recent activity by Yu-Chern Peh-
Hi Kuntal, L515 camera is not designed to work in space. The ideal environment for L515 camera to operate is indoors or in controlled lighting conditions only. Regards,Yu Chern
-
Hi Kuntal, L515 is designed to be used in indoors or in controlled lighting conditions. Hence it does not perform in space. Regards,Yu Chern
-
Hi Kuntal, Infrared light from the sun can interfere with the performance of the L515 which can degrade the quality of the depth images when used outdoors. As a power efficient LiDAR camera, L515 w...
-
Hi Kuntal, The ambient temperature range when L515 camera is streaming is 0-30 °C. Hence L515 camera is not designed to work at space. Regards,Yu Chern
-
Hi Dave, Yes, D455 and D435i camera do not have built-in support for pose stream data.(position and angle). There are a range of ways to obtain pose of the camera or of an observed object though. T...
-
Hi Nehalkabir02, The first thing to try is flipping the USB-C connector into the camera and inserting it the opposite way to change its polarity. Please ensure that you are connecting L515 came...
-
Hi Dave, The suggested alternatives for T265 are D455 and D435i. These cameras include an IMU, which is necessary for SLAM and tracking applications. Additionally, they require using 3rd party SL...
-
Hi Fatemeh Najafi, Thanks for reaching out to us. First of all, we would to declare that we had been discontinued our Tracking Camera, T265, starting February 2022. Hence, some content and the code...
-
Hi Jesus Dovale, Our GitHub collaborator has provided suggestion in the following discussion. Regards, Yu Chern
-
Hi Mozbayrak29, We are sorry to inform you that this channel is for Intel® RealSense™ products. Regarding your query, I would suggest you post your question on the Processors forum (https://communi...