RealSense Support

Position Tracking & the T265

Comments

4 comments

  • Yu-Chern Peh

    Hi Dave,

     

    The suggested alternatives for T265 are D455 and D435i. These cameras include an IMU, which is necessary for SLAM and tracking applications. Additionally, they require using 3rd party SLAM system. We suggest you use Spatial Intelligence SDK from SLAMcore.

     

    Here is some information that will be useful to you:

     

     

    Regards,

    Yu-Chern

    0
    Comment actions Permalink
  • Dave M Moore

    Thanks Yu-Chern,

    As far as I am aware the D455 and D435i do not output positional data. Can you confirm this please?

    Regards,

    Dave

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Dave,

    Yes, D455 and D435i camera do not have built-in support for pose stream data.(position and angle). There are a range of ways to obtain pose of the camera or of an observed object though. Therefore, they require using 3rd party SLAM system.

     


    Regards,
    Yu-Chern

    0
    Comment actions Permalink
  • Dave M Moore

    Yes, but the whole point of the processor on the T265 is that it does the processing for you. ie. your host computer doesn't need to do it. Are we saying that none of the current RealSense offerings support native 6-DoF tracking?

     

    0
    Comment actions Permalink

Please sign in to leave a comment.